This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/WEBENCH-POWER-DESIGNER: different result between TPS54340 and TPS54560

Part Number: WEBENCH-POWER-DESIGNER
Other Parts Discussed in Thread: TPS54560, TPS54340, TPS54540, TPS54360

Tool/software: WEBENCH® Design Tools

We designed with TPS54340 and TPS54560 by WEBENCH.

Vin: 32V to 40V
Vout: 24V
Iout: 3.3A
TA: 60 degC

The device characteristics is almost same between TPS54340 and TPS54560. However WEBENCH result was different.
We can designed with TPS54560, however we cannot design with TPS54340 because IC Tj is over 150 degC.
Why does these difference come?

Our customer is considering to use TPS54340 or TPS54560.
Should we select TPS54560 from WEBENCH result? Do you think we can use TPS54560 for the above using condition though output is high power?


Best Regards,
Kohei Sasaki