Part Number: PMP4311
Hi,
I want to create an interleaved PFC stage 3kW following the topology of the PM4311. I see that a flyback topology provides +12V of power supply. The flyback is insulated, but the entire project is not insulated (grounds are common). Can I use the +12V of the flyback to supply external devices like display? I need an insulated +12V and I don't want to create another supply or change something in the topology.
Do you have any suggestion?
thank you and best regards,
Andrea C.