This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP40025: flyback converter output voltage control

Part Number: PMP40025

I am working on PMP40025 48V fly back converter. I used the gerber files from TI and same equivalent values as given in design. Based on the calculations I made transformer. I have designed the transformer to work in 85Vac to 265Vac.

The converter works and produces 52V. How this 52 Voltage can be controlled to 48V + 1V. 

Whether controlling voltage sense resistors will control output voltage. Pls explain