This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TINA-TI or Spice Models
This is with reference to series of nice articles written by Ian Williams regarding SPICE model verification with respect to Datasheet results. I tried to simulate the circuit used as an example by him in his post, but was not getting the expected result. You can read his article and my post in comments section at the link provided below.
It could be some silly mistake I might be doing, but I found article to be useful enough in order to make sure I completely understand it.
I have also attached screenshot of the error I am getting, it also contains the circuit diagram.
Link for article: https://e2e.ti.com/blogs_/b/analogwire/archive/2017/07/27/trust-but-verify-spice-model-accuracy-part-1-common-mode-rejection-ratio-cmrr
Prasad,
Your differential setup has no input as the two controlled sources both have zero gain. Please set both to 0.5 (for a total of 1) and try again.
Regards,
JC
Hi Prasad,
JC's suggestion is exactly right. If you set the gain of your sources VCVS3 and VCVS1 to 0.5 (500m), you can use post-processing to extract the CMRR without seeing the divide by zero issue. In this case the CMRR of the OPA2137 model is equal to 89 dB, a bit off from the typical spec of 84dB. The -20dB/decade roll-off in the model also doesn't begin until high frequencies, while in the actual part the rolloff starts around 100 Hz. As you can now see, this model is quite old and not as accurate as those for our more recent devices.
Best regards,
Ian Williams
Applications Engineer/SPICE Model Developer
Precision Amplifiers