Part Number: TINA-TI
Other Parts Discussed in Thread: THS4140
Tool/software: TINA-TI or Spice Models
Hi,
I have used TINA-TI simulating basic behavior of THS4140 and getting results which are different than expected.
I would like to know about accuracy of the modelling, as shown by simulation results.
Example 1- Gain is supposed to be 10, according to device recommendation, yet I get different value (9.97). Simulation conditions are ideal, so only device parameters should affect results.
Example 2 - checking for device parameter of Vos (input offset voltage), specified by datasheet between 1 and 7mV, yet in simulation I see absolute zero
These are a few examples, and not clear to me whether the specific device model accurately reflects device parameters?!
How can I confirm?
Thanks,
Arie