This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TINA-TI or Spice Models
Hi,
I have the free version TINA-TI v9 and I cannot create a new macro for the attached circuit. The idea is to create a block to use in another circuit.
When I try to create a new macro using Macro Wizard, the option "Current circuit" is not available. Can someone please explain me how can I proceed or create the macro and send it?
Thank you very much,
Joaquim Santos
Joaquim,
You can use TINA9-TI to create a macro from a Spice netlist.
The procedure is given in the attached application note.
Creating a macro from a schematic is not a supported feature in TINA9-TI.
It is supported by TINA Industrial, which is available from Designsoft.
Regards,
Johnslva527[1].pdf