This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TINA-TI or Spice Models
Hi Team,
Is it possible to change a setting in TINA so that I can get a Bode plot with actual magnitude on the y-axis instead of dB? I would like to see the actual level response vs the normalized response.
Thank you!
Jared
Jared,
Double-click on the vertical axis of the plot and the Set Axis window will appear.
In the Scale pull-down on the lower left you can select Linear-dB, Linear or Logarithmic.
Select the one you want, and it will re-scale the vertical axis accordingly.
Regards,
John