can we enhance the output from 4 Amps to 8 Amps with almost same efficiency.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Amit,
While it is certainly possible to design a flyback with 8A output, this would not be the design to use as a starting point.
The transformer would need to be completely changed.
The output rectifier needs to be synchronous instead of a diode.
The wide input range is also going to be a problem.
A couple of options that can give you an example of what the circuit would look like
Thanks,
Robert