This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
Hello,
In order to avoid the requirement for Flash I am using the iPad version of Webench. However, recently I have encountered an error when trying to use the website. When trying to create a new design the page alternates 2 or 3 times a second between this:
and this:
Looking at the developer console it appears that during the transition between the two there is an error: "sitesearch-header-min.js?versionNumber=1.2:762 Uncaught ReferenceError: linkSearch is not defined at sitesearch-header-min.js?versionNumber=1.2:762"
I've tried different browsers, different computers, etc and it doesn't seem to work on any of them.
Any ideas on what's going on / how I can fix it?
Thanks,
Kyle Goodrick