This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP11600: Surge Protection - Voltage

Part Number: PMP11600

In the design : High Efficiency Universal AC Input to 5V 2A Adapter Reference Design

Is there any need for voltage surge protection device at the start of circuit? Similar to MOV or TMOV. We are planning to use the devices in India where there seem to quite some power fluctuations in the grid. Is such a additional protection indeed necessary/sufficient?