Part Number: TIDA-01167
Other Parts Discussed in Thread: LM5060
Dear Sir,
Please you kindly help check bewlow TIDA-01167 issue.
1. Fig27: do ISO7637-2 Pulse 1 test by 12V input voltage.
I saw output drop to -3.37V then to zero, does input voltage shutdown or LM5060 do output shut down for detect a fault condition?
2. If Fig27: ISO7637-2 Pulse 1 do test by 24V input voltage, It is same shutdown ?
Thanks
Steven