This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What are the benefits of using ISO1541 (Low-power, Bi-directional I2C Isolator) in the implementation of low cost, high efficiency communication modules used in Industrial applications like UPS and Energy Storage banks?
TIDA-01281 is a TI Reference Design solution to help develop low cost, high efficiency, isolated RS-485, I2C & CAN communication modules, that are used in industrial applications like UPS and Energy Storage banks.
ISO1541 is a low-power, bidirectional isolator that is compatible with I2C interface. This device is tested to provide isolation of 2500 VRMS per UL 1577 standard, with a transient immunity of 50kV/uS. In TIDA-01281, this device helps in communicating with other I2C enabled devices in a noisy environment, with the isolation barrier providing the ability to limit the noise from entering the main system ground and increasing the system immunity to noise.
For additional information about this topic, please refer to section 2 "Communication in Power Supplies" of the User Guide for TIDA-01281.
You can also download the design files (BOM, Schematic, Gerber) for this reference design from the TIDA-01281 folder.