This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/THS3491: Error caused by incompatibility between THS3491 device model and Tina macro-model extraction

Part Number: THS3491
Other Parts Discussed in Thread: TINA-TI, , LMH5401

Tool/software: TINA-TI or Spice Models

This is a software bug - probably in Tina. I follow your instructions and correctly extract a THS3491 Spice file from the Tina Macro-model. However the spice model is broken and does not work like an op-amp. If I set it for gain of +2 with a 1 Volt input and bipolar +/-15V the simulation tells me the output is 15 Gigavolts. If I make it a unipolar design then it gives me a 7.5V DC output voltage with spikes corresponding to the input pulse edges. To prove that it was Tina and not me doing something wrong I repeated the process for a different device macro-model and it worked perfectly ! Can you please address this promtly because I cannot simulate this part for my new design without a working P-Spice model. Thanks Steve