Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Hi all
I am using the THS3491 possibly in a 2 stage configuration to read signals out of Silicon photo multiplier (SiPM).
The SiPM is on a dev board and its output is coupled to a transformer (part number RFXF9503) as shown here
How do i add this transformer in TINA?
According to the SiPM's datasheet the inductor is used for impedance matching at 50 ohm so standard oscilloscopes can be used for readout
All ideas are appreciated
Thanks