This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LMK03328: Defalt VCO gain setting does not match the value in the data sheet.

Guru 19785 points
Part Number: LMK03328
Other Parts Discussed in Thread: LMK03318

Tool/software: WEBENCH® Design Tools

Hi Team,

When I run LMK03328 simulation, I found that WEBENCH uses VCO Gain = 49.011MHz/V as default value. However, the datasheet states VCO Gain = 55MHz/V (TYP).

Why does WEBENCH use 49.011MHz/V ? Is it considering the VCO Gain process variation ?

Please correct this value if this is a typo.

* LMK03318 simualtion is also using the similar value.

LMK03328 WEBENCH simulation default VCO Gain is 49.011MHz/V]

LMK03328 data sheet specification is 55MHz/V (TYP)

Best Regards,

Kawai