This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
Hello!
I'm trying to get +/-12V (3A) using LM5088. For -12v there is no problem, Webench creats the circuit but for +12V i get constat errors saying ' something went wrong'. When i change the output to 5V it creats the circuit.
Vin,min:12V
Vin,max:24V
Vin,nom,15V
Vout:12V
Iout:3A
Is there any other IC that i can get +12V and -12V? Not at the same time. Using different LM5088 IC in different circuits. Thanks.