Other Parts Discussed in Thread: PMP30168, INA198
Dear Sir
Good day! There are DC-DC power requirement for printer power and need IEC60950 LPS(Limit power source) . Spec as below.
1.Vin: 12-48V
Vout: 8.3V/5A
OCP :6.5A arround Peak load :20A at 1mS
2.Peak load mode:20A continue 1mS,0A 1.3mS,this mode must keep work 500 second。
3.Product need meet LPS
I find PMP30464 interleaved buck converter can meet the peak power but i dont know if it can meet IEC60950 LPS. if not , how to implement this function.
Regards
Tiger