This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TINA-TI or Spice Models
Hi dears
I want to use LF356 in my simulation project with OrCAD capture software, so I downloaded the LF356 library from ti.com and produced its library as reveal that described in the below link:
electronics.stackexchange.com/.../how-to-import-pspice-model-into-orcad-capture
than I add LF356 library to my project. After this the component that I see was as the below picture:
as you see the component has 5 pins that named 1, 2, 99, 50, 28. if we assume that this 5 pins are the main pins of an op-amp (negative input, positive input, output, negative supply, positive supply) witch pin is correspond to component pins? in other word i dont know what is the action of component pins.
thanks for your attentions.