Part Number: LM5175
Other Parts Discussed in Thread: LM5157
Tool/software: WEBENCH® Design Tools
Dear Sirs
Use LM5175 in the following project:
I enclose schematic and pcb in pdf format
VIN range 12-30V Vout 28V 15A 100Khz with a parallel of two inductor wurth 7443641000 10uH 37A 2.4 mOhm equivalent inductor 5uH 74A 1.2 mOhm.
With 13.5 V in input and 28 V in output the card works in buck-boost instead of working only in boost mode.
I think the main problem is that we developed it on 4-layer FR4, therefore the mosfet dissipation area does not allow to have short gate tracks.
One thing I checked between redoing the same project with the "LM5175 Buck-Boost Quickstart Tool - r9.xlsm" and with the "WBdesign" I get different results.
For example the compensation components (COMP pin) with the "WBdesign" I get 10Kohm + 15nF // 330pF with the "Buck-Boost Quickstart Tool - r9.xlsm"
I get 3K16 Kohm + 12nF // 39pF (NB by entering data of the inductance 5uH 1,2mOhm).
Another mistake we made is that of not having drawn tracks SW1 // HDRV1 and SW2 // HDRV2 side by side.
I would appreciate you to report any corrections before producing the next sample.
Best Regards
Orfeo MilaniSchematic Power.pdfPCB layout.pdf