Other Parts Discussed in Thread: LM5119,
Per reference design PMP10979 using LM5119 in parallel, is there a recommended add-on circuit perhaps to the FB2 node that allows some limited output voltage adjustment from 5V to 12V at maximum current of 45A? The add-on circuit is to be control through a voltage of 0-5V.
my application has a max 24V dc input but it requires an external control voltage (0 to 5V ) to adjust the output voltage from 5V to 12V. Any suggestions? thanks