This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
Dear TI Team,
I have designed a Flybuck converter for 44Vin to 54Vin at 12Vout-iso, 1.2A using Webench. kindly find the design report in attachment, in order to get 12V output i have changed the values of rfbb and rfbt resistors , while operating at 44V initially the circuit works and shows the desired output voltage but after few cycles the switcher ic's pin (ie Vin and gnd) is getting shorted internally. kindly address me what possibly could be the reason. Final_48V-to-12V_Converter-7_Nos.pdf
Hi,
Do you use the same transformer part number that is recommended by webench?
Also, do you test this on our EVM?
Thanks
-Arief
Hello Arief,
yes, I have used the same transformer part number that is recommended by webench, the green waveform shown in the attached image is the voltage across the primary side of the transformer which have oscillations while switching,could it be the reason?.output is 15V instead of 12V because i still have to size the values feedback resistors.
I have not tested in your EVM, find my schematic circuit in the attachment
I have designed pcb layout accordingly.
Regards,
- Alok
Hi Alok,
The switching in the transformer should happen because the transformer will transfer the energy to the secondary of the circuit.
Is the part damaged after loading at the primary or secondary?
Can you try to load the primary output voltage and ensure you maintain regulation and stability?
Also, it's a good idea to double check against an EVM and we can send you one if you prefer
Thanks
-Arief
Dear Arief,
I have connected my load at secondary in order to get isolated output, kindly explain me how connecting load in primary will ensure stability? I would like to cross check with your EVM, can I a get a sample.
Hi Alok,
On a flybuck design, the regulation happens at primary. Therefore i want to ensure stability first by trying to see if the primary side of regulation is ok.
If you have an address, i can send an EVM to you
Thanks
-Arief
Hi Alok,
No, i can send you one if you are located within the USA.
Just let me know your shipping address
Thanks
-Arief
Hi Alok,
Sounds great. I am glad that you are able to resolve the issue
Thanks
-Arief