Other Parts Discussed in Thread: UCC28711, LM5020
Hi,
I'm using this reference design for a flyback design. My input voltage is 100 to 1200 VDC. I have two questions:
First: I see D1 is 110V. So for the VOR I'm saying:
With two 800 V mosfets, let's leave 100V safety margin when at max voltage, so not to exceed 700V on each drain, i.e., in total 1.4kV.
Vinmax + Vz = 1400 + Vz <= 1200
Vz <=1400 – 1200 = 200V
Let’s pick Vz = 110V
Vz/VOR = 1.4 optimum ratio
VOR = 77 is this good?
Second: I replaced LM5020 with UCC28711 which max frequency is 100 kHz. I don't want to hit the minimum on time since I'm dealing with a wide input range 100 - 1200VDC and output windings 48V and 12V. Would UCC28711 work properly in this case?