Part Number: LM5161
Tool/software: WEBENCH® Design Tools
Hello,
I am trying to start a Webench design using LM5161, but I always get the same error: VoutPrim should be less than 0.5VinMin
My parameters are as follows:
LM5161 in a flybuck topology
VinMin = 45 V
VinMax = 67.2 V
Vout = 22 V
Iout = 0.4 A
IoutNom = 0.2 A
Tmax = 60 °C
Use ceramic capacitors and shielded inductors
Changing Iout, Tmax and options has no effect. The only way I have to let it work is selecting a Vout < 18 V, as if VinMin was the default 36 V disregarding my input.
Is it a bug or am I wrong in some way?
Thanks in advance.
Regards,
Stefano