This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TLV62585: TLV62585 don't simulate for 3.3V output

Part Number: TLV62585

Tool/software: WEBENCH® Design Tools

For some reason, Webbench will not simulate if I enter the below input for TLV62585.

Can't think of the reason why it will not simulate. 

TLV62585DRL
Input: 
DC 2.5 V - 5.5 V
Output: 
3.3 V at 3 A
Temp: 
30 °C

It said below.

Design cannot be created!

Your preferred device does not work with the inputs you selected.

Please change your inputs or select another device.