hello,
I have checked the document tidu304.pdf and have some related questions please.
what is the maximum load in mA of the circuit under rectified current input?
why is there a coil of 3.3uH (L3) in page 10 inserted before the buck stage?
what is the benefit of R75 and R87 in page 10?
It is mentioned in the document tidu304.pdf that the VA rating of the CT will be less by using higher voltage. I can't understand why. The one thing that I can see is that the capacitor after the MOS shunt will discharge in this case at high voltage and so the current can be less and so some losses are saved. But how the VA rating will be less is still unclear.
Last question is why to use the shunt mosfet while it seems that for higher values of C28, the voltage at the terminals of C28 seems not varying that much
Thank you very much.
Regards,
Amr Elhadidy