Tool/software: WEBENCH® Design Tools
Hi,
i want to see the transfer function from one point to another in a circuit. I use AC analysis, and can see the TF from source to point A, and source to point B. But i want to look at point A to point B.
Eg below i want to see the shape of this transformer, relative to a signal generator output (after 50 Ohm).
I can add a post-processor formula OUT(s)/IN(s) which seems to work, but this doesn't work with parameter stepping (unless i want to create multiple instances every time i change a component parameter sweep). Is there a way to do this?
I tried a controlled source with V(N1)/V(N2), but this is in time domain so doesn't work. Is there a simple way that im missing?