This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
David,
Thank you for your question, and your interest in Pspice for TI.
There are Cadence Pspice models built into the tool.
You can see them using the traditional Place Part panel.
You can more easily see them by clicking the Launch Pspice Part Search icon:
This will open a right-hand panel that displays a hierarchy of models.
The Texas Instruments folder holds the 5300+ TI device models organized in
the same way as presented on our web site. The other folders hold
the traditional Pspice primitives and models.
I hope this helps. Please let me know if you have any questions.
Regards,
John
Renato,
Thank you for your reply.
Please check for the following:
Thank you.
Regards,
John
Thanks, for taking the time to reply. Yes, I know about all he TI parts, that's a good thing. What I am asking about is the Cadence library, it has over 13000 models, which have all been vetted. You guys don't make power discrete's, and they're useful when modelling a power supply.
Thanks,
Dave Santos
David,
There is no way to add the commercially available Cadence libraries to Pspice for TI.
Cadence supports an upgrade path for the tool, but I'm not sure what that includes.
You can find out more about this option via the Upgrade button on the Pspice for TI Start Page.
There are a couple of alternatives to consider.
1. Pspice for TI contains a modelling application that allows you to customize some frequently used models.
The list includes a power MOSFET, power diode, L, C, sources, a transformer, and a switch.
If discrete MOSFETs are of interest, consider the parameterized power MOSFET model..
You can access it via the Modelling Application () and complete the GUI table to create a model customized to your favorite power MOSFET.
2. You can import models into the tool the usual way via the Tools/Generate Part menu.
The downside to this is that if the model is placed in schematic, it will be limited to plotting three waveforms in any sim.
Regards,
John
Thnks, John, I resolved.
It was a problem about "Home" directory (the user ambient variable).
Now it works.
Thank a lot.
Renato.