Part Number: EZ430-F2013
Hi Team,
Our customer would like to update the firmware version of EZ430-F2013 from 1.00.02.000 to 3.00.01. Is it updated thru CCS?
Regards,
Danilo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: EZ430-F2013
Hi Team,
Our customer would like to update the firmware version of EZ430-F2013 from 1.00.02.000 to 3.00.01. Is it updated thru CCS?
Regards,
Danilo
Yes, you could update through CCS. When you try to download and debug a project, it will prompt you to update the EZ-FET firmware.
You could also use a cloud tool like Uniflash and it will also prompt to update the EZ-FET firmware.
Hi Eddie,
Thank you very much for the confirmation and for your suggestion.
Regards,
Danilo
Hi Eddie,
We have received a feedback from the customer that he can't update the EZ430-F2013. According to the customer,
Thank you for support, but i cant run and update . This is my problem, MSP-FET430UIF JTAG TOOl dont upgrade. When i use code composer . Uniflash does not detect the device,
Here are the screenshot of device manager.
Regards,
Danilo
Danilo,
Do they also have a MSP-FET430UIF connected to the PC? I believe the EZ430-F2013 should show up as "MSP Debug interface", but this is a very old tool that I do not have to check myself.
If this is a COM port issue, they may want to try changing the COM port number.