Hello,
SDK: SimpleLink CC13x2 26x2 SDK - 5.20.00.52
I am trying to change the NPI in Host_test from default UART to SPI. I did not made any changes to the .syscfg Device Configuration.
But i tried to change the defines in ble5_host_test_cc13x2p2lp_appFlashROM_Release.opt
i edited:
-DNPI_USE_SPI
-DxNPI_USE_UART
-DNPI_FLOW_CTRL
-DPOWER_SAVING
But after that I got some errors.
the npi_config.h
So my question is. Are these the right defines to get SPI working? And do I need to define FLOW_CTRL and POWER_SAVING to use the MRDY and SRDY for SPI, or are they automatically activated with NPI_USE_SPI?
best regards,
Samuel