Part Number: CC2642R
Other Parts Discussed in Thread: CC2640, , SIMPLELINK-CC13X2-26X2-SDK, UNIFLASH
Dear support people,
We are using a custom board with a CC2642R (CC2642R1F) device. The board was originally designed for the CC2640 device and (via the CC2640R2) we have now replaced the processor with a CC2642R device. Hardware changes cf. SWRA582d (de-coupling) and SWRA495i (48 MHz chrystal) have been implemented.
I have had contact with Brian Zoro about this problem. Brian mailed me the following.
If not already done, please run the following tests:
- Try to flash the unmodified simple_peripheral (without OAD) example from SDK 6_20
- Try to flash the simple_peripheral_oad_(on|off)chip example from SDK 6_10 (without forgetting the BIM project )
- Make sure to share these results on E2E at the same time as the rest of their results.
I informed a colleague from the product line and he will take care on e2e meanwhile
Bullit 1
With regards to the first bullit, I added the "simple_peripheral_CC26X2R1_LAUNCHXL_tirtos7_ticlang" example from the SDK v6.20 to my workspace, but after flashing the device, CCS v12.0.0.00009 crashes! I have reported this via the "Crash Reported" dialog that pops up the next time I start CCS. Note that CCS does _not_ crash on the examples from SDK v5.20.
Note the CCS crashes both when I debug the program and when I load the program to run it stand-alone. The flasher, via the XDS110 debugger/emulator, finishes but -apparently- the program does not start. Also, when flashing, the progress is preceeded by a text "PT_LOAD"; I don't see that prefix when I flash an SDK v5.20 program (or a v6.10 "ccs" project, for that matter).
Bullit 2
The SDK v6.10 project "simple_peripheral_oad_onchip_CC26X2R1_LAUNCHXL_tirtos_ticlang" also crashes CCS v12.
The project "simple_peripheral_oad_onchip_CC26X2R1_LAUNCHXL_tirtos_ccs" from SDK v6.10 runs normally, when connected via the XDS110 (I programmed the device with the "Flash" button in CCS). However, when I remove the XDS110 and power cycle the board, it does _not_ run.