Other Parts Discussed in Thread: CC2650, SIMPLELINK-CC2640R2-SDK, LAUNCHXL-CC2650, CC2642R, CC2640R2F, BLE-STACK
My goal is to setup a simple peripheral and central using ble5stack to test the coded PHY and extended advertising.
I’m able to use my old launchpad to download and debug the simple peripheral app and now in the process of setting up another (new) launchpad to run the simple central and ran into some issue with the new launchpad. My old and new are the same CC2650 launchpad Rev1.3 and all jumpers are the same.
The old launchpad is able to download and debug as normal, but the new launchpad doesn’t stop at main after the flash download and landed in “NORM_ThisLibraryIsFor_CC26x0R2_HaltIfViolated: area…
I have upgraded the new launchpad to the same firmware 3.0.0.13 same as my old one :
<<<< Device 0 >>>>
VID: 0x0451 PID: 0xbef3
Device Name: XDS110 Embed with CMSIS-DAP
Version: 3.0.0.13
Manufacturer: Texas Instruments
Serial Num: L1002678
Mode: Runtime
Configuration: Standard
Switching device into DFU mode.
I am using the IAR 8.32.2, SDK 4.10.0.10, xdctools 3.51.03.28_core
Is there something else I need to download to the new launchpad for it to run ?