Hi,
After the IOS active disconnection, a Write Transaction will be sent, and then connecting with an Android phone will result in a failed service discovery issue
In addition to the Android connection will find that the service fails, do the host to connect to the slave, call GATT_WriteNoRsp returns 0x16, call GATT_ExchangeMTU interface returns 0x16, it will affect the arbitrary ATT commands sent
SDK:simplelink_cc13xx_cc26xx_sdk_7_10_01_24
examples:multi_role
Problematic cell phones:iPhone 13(IOS15.2.1)、iPhone 14 Pro(IOS16.5)
Android phones don't have this problem with active disconnects