Other Parts Discussed in Thread: SYSCONFIG
Hello, TI Team.
I am using CC2340R5 as the central device for transparent transmission with peripheral devices that are also CC2340R5. The peripheral sends about 30 bytes of data to the central device every 500ms, at which point the MTU is a maximum of 251 bytes.
When the central device receives about 1800 bytes of data, the central device appears to no longer receive the data transmitted by the peripheral device, and the peripheral device continues to transmit data. I tried several times with the same result.
The code below is where the data is finally received, printed to the PC via the serial port.

My colleague had the same problem.
Best Regards,
Joey.