This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
HI,
We have to use CC2340R5 as central mode and same device (CC2340R5) using as peripheral mode, we need to connect to peripheral device (it act as key fob) and central device (Instrument Cluster) how to connect peripheral central device to the peripheral using Discover Service UUID of the peripheral device.
Note: Above same functionality we tried using CC2642R1 device using SDK (simplelink_cc13xx_cc26xx_sdk_7_10_01_24) it is working fine.
But how to do same functionality using CC2340R5 device using SDK (simplelink_lowpower_f3_sdk_7_40_00_64) and what changes required in the system configuration of the central device configuration using (CCS 12.4 version)
Please provide some documentation and which steps we need to fallow
thanks, and regards
Balaji Wankhede
Greetings Balaji,
I am currently looking into this, and will get back to you as soon as possible. Thank you for your patience.
Best,
Achyut Ray