Part Number: CC2674R10
Other Parts Discussed in Thread: SN74AVC2T244
Tool/software:
I'm working with a customer who is using the SN74AVC2T244 as a level translator between another MCU and the CC2674 device. We are finding that the drive strength of the level translator is quite high, and this is causing ringing at the input of the CC2674. The overshoot is around 4.11V and the undershoot is around -1.41V. The VDDS I/O rail used for the CC2674 is nominally 3.3V.
This technically violates our datasheet specs, but only persists for ~7ns. We are wondering if this should be a concern that would prematurely wear out the CC2674 device. The obvious solution would be to add some small series resistance near the level translator, but the customer is trying to avoid an unnecessary board spin if possible due to a very tight production timeline. Please see the attached scope images:




Thanks,
Stuart