Part Number: CC2340R5
Tool/software:
I am having a lot of problems with timing accuracy using the CC2340R5 and BLE Stack.
I have managed to configured DIO19 to output the 48Mhz / 8 = 6Mhz to try and validate the underlying the clock frequency.
This seems to vary from 6.0007 Mhz to 5.952 Mhz. I am really trying to setup this Application to perform some realtime processing, hence I am looking for accurate time domain.
A few questions on this device which I can't work out from the Datasheet.
1) Does the ARM core actually run of the HFEXT 48Mhz crystal - or does it always using the less accurate internal RC Oscillator?
2) I've tried utilising the HFXT Cap Array adjustments - but no real change with those. The reference design from TI shows not to use load capacitors on the crystal itself, maybe I should just try that.
Any support on this would be really helpful.
For anyone else trying to output the clock here is the code snippet I've used. (Placed after Board_Init() )
/* Start of 48Mhz CLK Debugging */
// drive output low first
GPIO_setConfig(19, GPIO_CFG_OUTPUT | GPIO_CFG_OUT_LOW );
// Conigure the IOC.IOC19 PORTCFG MMR to seelct DTB
HWREG(IOC_BASE + IOC_O_IOC19 ) &= ~IOC_IOC19_PORTCFG_M ;
HWREG(IOC_BASE + IOC_O_IOC19 ) |= IOC_IOC19_PORTCFG_DTB ;
//
HWREG(IOC_BASE + IOC_O_DTBCFG) &= ~IOC_DTBCFG_ULLSEL_M ;
HWREG(IOC_BASE + IOC_O_DTBCFG) |= 0x1 << IOC_DTBCFG_ULLSEL_S ; // 0x1 to route CLKD to DTB0
// Enable IOC.DTBOE.EN0
HWREG(IOC_BASE + IOC_O_DTBOE) &= ~IOC_DTBOE_EN0_M ;
HWREG(IOC_BASE + IOC_O_DTBOE) |= IOC_DTBOE_EN0_EN ;
// Seelct which clock (CKMD) to output on DTB0 (DTB[0])
HWREG(CKMD_BASE + CKMD_O_DTBCTL) &= ~CKMD_DTBCTL_CLKSEL_M ;
HWREG(CKMD_BASE + CKMD_O_DTBCTL ) |= (clockSrc) << CKMD_DTBCTL_CLKSEL_S ;
// enable DTB Output
HWREG(CKMD_BASE + CKMD_O_DTBCTL) &= ~CKMD_DTBCTL_EN_M ;
HWREG(CKMD_BASE + CKMD_O_DTBCTL ) |= CKMD_DTBCTL_EN;
/* End of CLK Debugging */