I am using Packet sniffer with CC2540 USB dongle. However, the documentation of the software is not very clear for me in many cases.
Regarding this post http://e2e.ti.com/support/low_power_rf/f/538/p/106575/376118.aspx#376118 I am still wondering how to know which packet is sent by which side? I see the answer to the thread but it is understandable when two L2CAP-C packets are sent within one connection event. I attached the screenshots of 4 more cases. In all cases 4 packets are sent in one connection event
1- In the first case, 3 of the packets are L2CAP-C and 1 is L2CAP-S packets (Btw, -C is probably Control but what does (L2CAP)-S refer to?). So I am confused about what do these first 3 L2CAP-C packets tell to me? Which one is sent by the master and which one(s) are from slave?
2- In the second case, the third L2CAP-C packet has an FCS error. So what should I understand from that? Is it a packet that has sent from slave or master? What happened to this packet and what was its purpose to be sent? Since it has an error will it be re-sent?
3- In third case all of the packet types are L2CAP-C so the PDU length is 0. Which ones belong to master and which ones belong to slave? Why 4 L2CAP-C packets are sent at one time? What is the purpose of sending 4 of them at one time if the PDU is 0?
4- In the last case there are 2 notifications in one connection event. These notifications are supposed to be sent periodacllay per one second as I programmed so. How come two sequential notifications are sent in one communication events? What do the other L2CAP-C packets stand for? Are they ACKs?
5- My last question is about ACK messages. I know that notifications do not expect confirmations from the master. But as far as I know this is a Stop and Wait - ARQ protocol. So the sender doesn't send any further frames until it receives an (ACK) signal. DO we see the ACK messages in Packet Sniffer?
I know it is a long post but if you could answer some questions I am sure you will contribute to knowledge of many of other readers.
Thanks!