This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm trying to program the chip CC250, using the mini development Kit .
I started with the Flash programmer selecting the flash image that is in the directory C:\Texas Instruments\BLE-CC254x-1.2.1\Accessories\HexFiles\CC2540MiniDkDemoSlave.hex. Then, I selected 'Erase, program and verify' But it doesn't work. An error is shown after 'Perform action'
CC2540 - ID4869: HEX file content at address 0x1CC7A exceeds chip's 16 kB flash size.
I've tried with the other hex files that I found in the same directory.
Thank you in advance for your help
This error message typically occurs if the SmartRF Flash Programmer is not receiving the expected response from the device.
Normal causes for this are:
Br,
ABO
Hello everyone,
Thank you for your help. I've already resolved the problem. Exactly as you mentioned the issue was that the keyfog wasn't doing powered although in the cc debugger always showed the green led! I just cleaned the negative terminals of the battery with a fine sandpaper and that was all. :)
Bye.