Other Parts Discussed in Thread: CC2540, BLE-STACK
Hi everybody!
I've just purchased Connect Blue OLP425-16i, with CC2540 installed on it.
The problem that is frustrating me is the CC Debugger, with red LED on.
I followed this manual, in order to start programming the module:
http://support.connectblue.com/display/PRODBTPLA/cB-OLP425+Development+Kit+Getting+started
As suggested, I installed BLE-STACK, extracted SDK for OLP425 inside the BLE-STACK folder.
As it showed on the picture below, through USB I connected my CC Debugger to the adapter board with JST output and I connected it to the module.
The Adapter board is provided by Connect Blue. JST/JST cable is the simple crossover cable which I purchased from the local store.
My CC debugger could be seen on the TI Flash Programmer, where I updated it's software, however the red LED is still on.
The OLP425-16i should start the pre-loaded demo application, when the power is connected and blink it's green LED, but it does not.
Moreover BLE-Stack cannot recognize the COM port, showing that there are no ports connected. However, when I try to connect my Arduino to the same port it is recognized.
What am I doing wrong?
The main problem for me is that there is no proper step-by-step guide, which I can follow.
ps. My OS is Windows 7, 64 bit.