Part Number: CC2540
Other Parts Discussed in Thread: CC2650
I am trying to debug using the CC debugger and CC 2540 USB Dongle. I get the following error when I try to connect. I do not see and XDS110 in the Ports under Device Manager. I do see CC Debugger and CC2540 USB Dongle under Cebal controlled devices.
Error connecting to the target:
(Error -260 @ 0x0)
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the ReadMe.txt file there
for instructions.
(Emulation package 6.0.628.1)