Hello,
I'm working on a Bluetooth low energy application based on a BLE112 modem, and MSP4302416 processor. As described in BLE112 datasheet, we have had a TPS62733 regulator with a 2.3V output. Furthermore in our application, we used a ADC that needs at least 3.0V power supply.
I cannot power the whole circut through the TPS62733, because the ADC will not work properly at 2.3V. In the same manner, if I supply the BLE112 through the TPS62733, I will get voltage level mismatch between MSP430 (3.0V), and BLE112 (2.3V). Using level shifter is excluded.
So my questions are :
1) - What is the exact role of the TPS62733 for the BLE112? And can we really get a 20% energy saving when using 2.3V, instead of 3.3V?
2) - When supplying the BLE112 through TPS62733, what is the output level of Tx/Rx/CTS/RTS and other GPIOs?
3) - Same question, when bypassing TPS62733.
4) What is the MSP430 impact of power supply voltage drop (glitches ?) on a running code?
5) All the application notes that suggest to use a TPS62733 work in standalone (no additional CPU). So when using an additional MSP430 with a 3V power supply (for the whole design), what are the real benefits of a TPS62733?
Thank's in advance
Regards
pazcal