This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI engineers and Forum members,
Please help. I'm trying to send data out of P1_6 [TxD] (USART1, Alt.2) but do not see any activity at the port. I've set breakpoints at UxDBUF and the line after [in BOLD] in the UART Transmit Interrupt [halUartTxIsr] below, stepping through the code in the Disassembly window, while monitoring the U1DBUF and Basic Registers. I'm using the cc2541 Keyfob and cc2540 USB Dongle.
[--Begin code--
/***************************************************************************************************
* @fn halUartTxIsr
*
* @brief UART Transmit Interrupt
*
* @param None
*
* @return None
***************************************************************************************************/
#if (HAL_UART_DMA == 1)
HAL_ISR_FUNCTION( halUart0TxIsr, UTX0_VECTOR )
#else
HAL_ISR_FUNCTION( halUart1TxIsr, UTX1_VECTOR )
#endif
{
HAL_ENTER_ISR();
if (dmaCfg.txHead == dmaCfg.txTail)
{
IEN2 &= ~UTXxIE;
dmaCfg.txMT = 1;
}
else
{
// UTXxIF = 1;
UTXxIF = 0;
UxDBUF = dmaCfg.txBuf[dmaCfg.txHead++];
if ((HAL_UART_DMA_TX_MAX != 256) && (dmaCfg.txHead >= HAL_UART_DMA_TX_MAX))
{
dmaCfg.txHead = 0;
}
}
HAL_EXIT_ISR();
}
#endif
/***************************************************************************************************
* @fn halUartTxIsr
*
* @brief UART Transmit Interrupt
*
* @param None
*
* @return None
***************************************************************************************************/
#if (HAL_UART_DMA == 1)
HAL_ISR_FUNCTION( halUart0TxIsr, UTX0_VECTOR )
#else
HAL_ISR_FUNCTION( halUart1TxIsr, UTX1_VECTOR )
#endif
{
HAL_ENTER_ISR();
if (dmaCfg.txHead == dmaCfg.txTail)
{
IEN2 &= ~UTXxIE;
dmaCfg.txMT = 1;
}
else
{
UTXxIF = 0;
UxDBUF = dmaCfg.txBuf[dmaCfg.txHead++];
if ((HAL_UART_DMA_TX_MAX != 256) && (dmaCfg.txHead >= HAL_UART_DMA_TX_MAX))
{
dmaCfg.txHead = 0;
}
}
HAL_EXIT_ISR();
}
#endif
--End code--]
U1DBUF stays at 0x00 even though each byte of the data message can be seen, being built in the Basic Registers and written to U1DBUF one at a time. Is there a specific condition that needs to be met before a byte of data written to U1DBUF is seen in the register?
Any help is appreciated. Thanks.
Regards,
Dag
I'm using the following settings:
1) Preprocessor defined symbol used is HAL_UART_DMA=2.
2) I added a line of code to set P1_6 today (see below)
3) A scope probe is set at the Keyfob's Buzzer [B2:1] to monitor the P1_6 output.
[--Begin code--
static void HalUARTInitDMA(void)
{
halDMADesc_t *ch;
#if (HAL_UART_DMA == 1)
PERCFG &= ~HAL_UART_PERCFG_BIT; // Set UART0 I/O to Alt. 1 location on P0.
#else
PERCFG |= HAL_UART_PERCFG_BIT; // Set UART1 I/O to Alt. 2 location on P1.
#endif
PxSEL |= HAL_UART_Px_SEL; // Enable Peripheral control of Rx/Tx on Px.
UxCSR = CSR_MODE; // Mode is UART Mode.
UxUCR = UCR_FLUSH; // Flush it.
P2DIR &= ~P2DIR_PRIPO;
P2DIR |= HAL_UART_PRIPO;
PxDIR |= 0x40; // #: [30Nov2015] Setup P1_6 as output
...
}
--End Code--]
After HalUARTInitDMA() executes this is the status of the registers.
Is the setup correct?
Hello Dag,
Yes, I think it should be possible.
I cannot see where you write to start the transmissions (write to U1DBUF or trigger dma transfer). Look more in details at the implementations in the following files:
C:\Texas Instruments\BLE-CC254x-1.4.1.43908\Components\hal\target\CC2540EB\_hal_uart_isr.c
C:\Texas Instruments\BLE-CC254x-1.4.1.43908\Components\hal\target\CC2540EB\_hal_uart_dma.c
Hello Eirik,
It's good to learn that P1_6 on the cc2541 Keyfob can serve as a UART TxD output, despite being physically connected to the buzzer [B2:1].
INT_HEAP_LEN=3072
HALNODEBUG
OSAL_CBTIMER_NUM_TASKS=1
HAL_AES_DMA=TRUE
HAL_DMA=TRUE
xPOWER_SAVING
HAL_LCD=FALSE
HAL_LED=FALSE
HAL_UART=TRUE
xHAL_UART_DMA=1
HAL_UART_DMA=2
xHAL_UART_ISR=0
HAL_KEY=FALSE
xNPI_UART_PORT=HAL_UART_PORT_0
NPI_UART_PORT=HAL_UART_PORT_1
NPI_UART_FC=FALSE
In reference to U1DBUF, I saw it was dereferenced to UxDBUF in _hal_uart_dma.c; so, I placed a breakpoint at
UxDBUF = dmaCfg.txBuf[dmaCfg.txHead++];
in the ISR code below--code execution does stop there. I was able to step through and observe the Basic Registers, to verify and validate the UART message I need to transmit out of TxD output port P1_6; however, P1_6 doesn't produce an output when it is probed with an oscilloscope at the buzzer [B2:1].
[ --Begin code--
#if HAL_UART_TX_BY_ISR
/***************************************************************************************************
* @fn halUartTxIsr
*
* @brief UART Transmit Interrupt
*
* @param None
*
* @return None
***************************************************************************************************/
#if (HAL_UART_DMA == 1)
HAL_ISR_FUNCTION( halUart0TxIsr, UTX0_VECTOR )
#else
HAL_ISR_FUNCTION( halUart1TxIsr, UTX1_VECTOR )
#endif
{
HAL_ENTER_ISR();
if (dmaCfg.txHead == dmaCfg.txTail)
{
IEN2 &= ~UTXxIE;
dmaCfg.txMT = 1;
}
else
{
// UTXxIF = 1;
UTXxIF = 0;
UxDBUF = dmaCfg.txBuf[dmaCfg.txHead++];
if ((HAL_UART_DMA_TX_MAX != 256) && (dmaCfg.txHead >= HAL_UART_DMA_TX_MAX))
{
dmaCfg.txHead = 0;
}
}
HAL_EXIT_ISR();
}
#endif
--End code-- ]
This prompts some more questions:
I'll await your responses. Thanks for you help.
Regards,
Dag
After adding HAL_UART_ISR=2 defined symbol to the list of Preprocessor Defined Symbols, the compiler returns the following warnings and errors.
Warning[Pe301]: typedef name has already been declared (with same type) C:\Texas Instruments\BLE-CC254x-1.4.1.43908\Components\hal\target\CC2540EB\_hal_uart_isr.c 204
Warning[Pe301]: typedef name has already been declared (with same type) C:\Texas Instruments\BLE-CC254x-1.4.1.43908\Components\hal\target\CC2540EB\_hal_uart_isr.c 210
Error[Pa052]: #pragma "call_graph_root" can only be used on a definition C:\Texas Instruments\BLE-CC254x-1.4.1.43908\Components\hal\target\CC2540EB\_hal_uart_isr.c 607
Error[Pe247]: function "halUart1TxIsr" has already been defined (at line 1016 of "C:\Texas Instruments\BLE-CC254x-1.4.1.43908\Components\hal\target\CC2540EB\_hal_uart_dma.c") C:\Texas Instruments\BLE-CC254x-1.4.1.43908\Components\hal\target\CC2540EB\_hal_uart_isr.c 607
Error while running C/C++ Compiler
Does this mean that HAL_UART_DMA=2 conflicts with HAL_UART_ISR=2 and needs to be removed from the Preprocessor list? Please advise.
Thanks for you help.
Regards,
Dag
Hello Eirik,
I've disabled the HAL_UART_DMA=2 Defined Symbol (please see Preprocessor list below) and now the compiler returns these warnings:
Warning[Pe301]: typedef name has already been declared (with same type) C:\Texas Instruments\BLE-CC254x-1.4.1.43908\Components\hal\target\CC2540EB\_hal_uart_isr.c 204
Warning[Pe301]: typedef name has already been declared (with same type) C:\Texas Instruments\BLE-CC254x-1.4.1.43908\Components\hal\target\CC2540EB\_hal_uart_isr.c 210
which points to TYPEDEFS in the _hal_uart_isr.c code file.
[--Begin code--
...
/*********************************************************************
* TYPEDEFS
*/
#if HAL_UART_ISR_RX_MAX <= 256
typedef uint8 rxIdx_t;
#else
typedef uint16 rxIdx_t;
#endif
#if HAL_UART_ISR_TX_MAX <= 256
typedef uint8 txIdx_t;
#else
typedef uint16 txIdx_t;
#endif
...
--End code--]
The Preprocessor Defined Symbols list is now:
INT_HEAP_LEN=3072
HALNODEBUG
OSAL_CBTIMER_NUM_TASKS=1
HAL_AES_DMA=TRUE
HAL_DMA=TRUE
xPOWER_SAVING
HAL_LCD=FALSE
HAL_LED=FALSE
HAL_UART=TRUE
xHAL_UART_DMA=1
xHAL_UART_DMA=2
xHAL_UART_ISR=0
HAL_UART_ISR=2
HAL_KEY=FALSE
xNPI_UART_PORT=HAL_UART_PORT_0
NPI_UART_PORT=HAL_UART_PORT_1
NPI_UART_FC=FALSE
How can I fix the warnings? Please advise. Thanks.
Hello Dag,
1. P1.6:
I meant that using P1.6 should work. But you might have to disconnect the buzzer as it might add some load to the line.
2. Warnings:
There are a lot of defines in the hal_board_cfg.h files that mess things up. However, before I continue, I would advice you to consider using the dma implementation instead of ISR as it is a more reliable solution. If you want to get rid of the warnings you have to remove all the HAL_UART_DMA and HAL_UART_ISR defines and just have the HAL_UART_ISR =2 in your projcet options->defines symbols. The warning comes due to the fact that HAL_UART_DMA gets defined with a non-zero value which in turn will add both the "_hal_uart_dma.c" and the "_hal_uart_isr.c" in the hal_uart.c file:
#if HAL_UART_DMA
#include "_hal_uart_dma.c"
#endif
#if HAL_UART_ISR
#include "_hal_uart_isr.c"
#endif
.....
3. CC2541/43/44/45 Peripherals Software Examples is standalone example code and is not a part of the BLE stack. The following are a part of the ble stack:
C:\Texas Instruments\BLE-CC254x-1.4.1.43908\Components\hal\target\CC2540EB\_hal_uart_isr.c
C:\Texas Instruments\BLE-CC254x-1.4.1.43908\Components\hal\target\CC2540EB\_hal_uart_dma.c
Hello Eirik,
Thank you. Following your recommendation about using HAL_UART_DMA=2, the cc2541 Keyfob now transmits a message from P1.6. For now, I'll keep the buzzer connected because the audible feedback is quite useful for my application.
On the other hand, the message transmitted from P1.6 is actually a command being sent to an external MCU, which needs to be transmitted continuously at 10Hz, as soon as the Keyfob pairs with the USB Dongle. Which example code can I modify to accomplish this task? Please advise. Thanks.
Hello Eirik,
That worked, thanks.
I have another issue. The message being transmitted is composed of two 8-bit tokens. The complete, concatenated message is being transmitted, however, the USART appears to be inserting a additional STOP bit between the first 8-bit and second 8-bit token. What could be causing this behavior?
For example, I need to transmit this message:
<START BIT><0x91><STOP BIT><START BIT><0x0D><STOP BIT>
The USART transmits the message this way:
<START BIT><0x91><STOP BIT><STOP BIT><START BIT><0x0D><STOP BIT>
The port is set for 9600 BAUD,n,8,1:
[--Begin code from npi.h--
#if !defined( NPI_UART_BR )
// #: [2Oct2015] Changed the baud rate to 9600 for transmission between the Host MCU and the cc2541
// #define NPI_UART_BR HAL_UART_BR_115200
#define NPI_UART_BR HAL_UART_BR_9600
#endif // !NPI_UART_BR
--End code from npi.h--]
[--Begin code from _hal_uart_dma.c--
UxUCR = UCR_STOP; // 8 bits/char; no parity; 1 stop bit; stop bit hi.
--End code from _hal_uart_dma.c--]
Thanks for your help.