This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to use LinuxSPPLE_PM of Bluetopia stack with CC2564

Other Parts Discussed in Thread: CC2564, CC2564MODA, MSP430F5438A

Hi, Everyone

I have a question about LinuxSPPLE_PM of CC2564 with AM335x and CC2564 with MSP430.

I setup these device:
(a)CC2564 + Linux AM335x
I watch this URL
processors.wiki.ti.com/.../Using_CC2564_with_Linux
but this URL is old version of Bluetopia stack.
I try ProcesserSDK 3.0 + TI-BT-STACK_LINUX-ADDON + patchfile

(b)CC2564 + MSP430
I try MSP430F5438A EVM + CC2564MODA.

I want to communicate between (a) and (b) with LinuxSPPLE_PM.

I got Log of AM335x + CC2564 (a)
===============================================================
SPPMLE>1 1

BTPM_Initialize() Success: 0.
DEVM_RegisterEventCallback() Success: 5.
SPPMLE>9 1

echo 117 > /sys/class/gpio/export
echo out > /sys/class/gpio/gpio117/direction
echo 0 > /sys/class/gpio/gpio117/value
echo 1 > /sys/class/gpio/gpio117/value
echo 0 > /sys/class/gpio/gpio117/value
echo 1 > /sys/class/gpio/gpio117/value
BT COMM PORT (/dev/ttyS1): 1
Changing HCI baud rate to 3000000
Status: Executing BTS Script /lib/firmware/TIInit_6.7.16.bts.
Status: BTS Script successfully executed.
DEVM_PowerOnDevice() Success: 0.
SPPMLE>
Device Powered On.
SPPMLE>RegisterGATTCallback

GATM_RegisterEventCallback() Success: 1.
SPPMLE>
Remote Device Found.
BD_ADDR: 0017E9E57B84
Device Name:
Device Flags: 0x80000000
RSSI: 0
Friendly Name:
App. Info: : 00000000
Paired State : FALSE
Connect State: FALSE
Encrypt State: FALSE
Sniff State : FALSE
COD: 0x001F00
SDP Serv. Known : FALSE
SPPMLE>
Remote Device Properties Changed.
BD_ADDR: 0017E9E57B84
Device Flags: 0x80000008
Connect State: TRUE
SPPMLE>
Remote Device Properties Changed.
BD_ADDR: 0017E9E57B84
Device Name:
Device Flags: 0x80000009
SPPMLE>
Remote Device Properties Changed.
BD_ADDR: 0017E9E57B84
Device Flags: 0x80000001
Connect State: FALSE
SPPMLE>
=====================================================================

and I got Log in CC2564 + MSP430 Case (b)
=====================================================================
SPP+LE>Client

******************************************************************
* Command Options General: Help, GetLocalAddress, SetBaudRate *
* Quit, *
* Command Options BR/EDR: Inquiry, DisplayInquiryList, Pair, *
* EndPairing, PINCodeResponse, *
* PassKeyResponse, *
* UserConfirmationResponse, *
* SetDiscoverabilityMode, *
* SetConnectabilityMode, *
* SetPairabilityMode, *
* ChangeSimplePairingParameters, *
* GetLocalName, SetLocalName, *
* GetClassOfDevice, SetClassOfDevice, *
* GetRemoteName, SniffMode, *
* ExitSniffMode, Open, Close, Read, *
* Write, GetConfigParams, *
* SetConfigParams, GetQueueParams, *
* DisplayRawModeData, AutomaticReadMode,*
* SetQueueParams, Loopback, *
* CBSend. *
* Command Options GAPLE: SetDiscoverabilityMode, *
* SetConnectabilityMode, *
* SetPairabilityMode, *
* ChangePairingParameters, *
* AdvertiseLE, StartScanning, *
* StopScanning, ConnectLE, *
* DisconnectLE, PairLE, *
* LEPasskeyResponse, *
* QueryEncryptionMode, SetPasskey, *
* DiscoverGAPS, GetLocalName, *
* SetLocalName, GetLERemoteName, *
* SetLocalAppearance, *
* GetLocalAppearance, *
* GetRemoteAppearance, *
* Command Options SPPLE: DiscoverSPPLE, RegisterSPPLE, LESend, *
* ConfigureSPPLE, LERead, Loopback, *
* DisplayRawModeData, AutomaticReadMode *
******************************************************************

SPP+LE>Inquiry

SPP+LE>
Inquiry Entry: 0x28B2BDEFCB16.

SPP+LE>
Inquiry Entry: 0x1040F3E68E74.

SPP+LE>
Inquiry Entry: 0x34C731AB40F6.

SPP+LE>
Inquiry Entry: 0xD03972CD8321.

SPP+LE>
Inquiry Entry: 0xE8B1FCCE5873.

SPP+LE>
Result: 1,0x28B2BDEFCB16.
Result: 2,0x1040F3E68E74.
Result: 3,0x34C731AB40F6.
Result: 4,0xD03972CD8321.
Result: 5,0xE8B1FCCE5873.

SPP+LE>Open 4 1
SPP_Open_Remote_Port success, Serial Port ID = 1.

SPP+LE>
SPP Open Confirmation, ID: 0x0001, Status 0x0002.

SPP+LE>
=========================================================================

Can you tell me how to use these BLE Demo program after this ?

I already see this manual for SPPLE.
wiki.tiprocessors.com/.../WL18xx_AM335x_TI_Bluetooth_Stack

but It is discribed between WL8 and iOS app.
I do not know how to set

Best Regards
Hiroyasu