Other Parts Discussed in Thread: TIDA-00690, , CC2560
Tool/software: Code Composer Studio
Hi,
I'm using the CC2650LounchPad development board.
I've implemented a prototype application base on TIDA-00690 Energy Harvesting for Wireless Switch Power Reference Design.
Concerning Firmaware, I started from Simple_Broadcaster_cc2650lp_app/Simple_Broadcaster_cc2650lp_stack.
I've configured ADV TYPE as ADV NON CONN IND, so that it works as beacon, only TX is activated in Adverstasing mode, while the Receiver is not in order to minimize the power consumption.
I'm able to send one ONE packet data on the three channel [37-38-39] both when I press the energy harvserter switch [AFIG-0007] and when I release.
I' would like to send at least TWO packet data on the three channel, both pressing and releasing the switch.
To do that, first I guess I need to reduce the ADV INTERVAL from 100ms to 10ms or around. I know that this is not compliant with BLE protocol, but I do not care.
If I simply try to change value in #define DEFAULT_ADVERTISING_INTERVAL 160, I have no effect. So, my question is how I can do that in Simple_Broadcaster_cc2650lp_app?
Furthermore, I reduce power consumption of Simple_Broadcaster_cc2650lp_app, reducing external Flash Memory consumprion according code modification described in SWRA478C.
Is there any other suggestion to reduce power consumption in this application with CC2650 LounchPad?
Thank you.
Kind Regards.
Paolo Garavaglia