Hi
At Motion data, the sensor value in the z direction is incorrect.
SensorTag is put on the table, therefore, I expect that all of xyz direction values are 0.
However, the result is x=0G, y=0G and z=4G.
- SensorTag software is ver2.2.2 (firmware1.5)
- Android application is v5.7.3(Build70)
If the SensorTag software is back to the older version 2.2.1 (Firmware1.4) then
the result become better (x=0G, y=0G and z=1G).
What should do I do?
Thanks and Best regards,
HaTa.