Part Number: SIMPLELINK-CC26X2-SDK
Hi,
When enabling scan and advertise simultaneously delays of up to 500 ms for sending advertisements were observed for advertising interval 100 ms. While pointed out that timing delays can occur trying to scan and advertise at the same time since the CC26x2 is trying to interleave advertising/connection events, reducing scan window and scan interval from 500ms to <100ms seems to mostly avert this issue. So is it right to conclude that during a scan window advertisements get blocked? While reducing scan window and scan interval to say 30ms is acceptable, will this increase chance for packet loss due to delay in channel switching or other delays during which device is not scannin, since these would occur much more frequently with the changes. Cant find any mention of delay between scan windows, is there any documentation, I'm assuming about 100uS. Also just to confirm during a scan window it scans in only one channel, i.e channel switching is window to window,right?
Thanks in advance