Other Parts Discussed in Thread: CC2640,
Hi:
At present,I has two demoboards, one with 32kHz crystal oscillator and one without.The demoboard with 32kHz crystal oscillator successful operation of simple_peripheral_oad_offchip. But the other one failed.
So I modify the simple_peripheral_oad_offchip to follow the RCOSC(http://www.ti.com/lit/an/swra499b/swra499b.pdf?tdsourcetag=s_pcqq_aiomsg:Running Bluetooth® low energy on CC2640 Without 32 kHz Crystal),But it still didn't work.
I wonder if it is necessary to use 32Kh crystal oscillator before using the function of OAD?
Please reply in your busy schedule. Thank you. Thank you very much.
chip: CC2640R2F
SDK:simplelink_cc2640r2_sdk_3_20_00_21
IDE: IAR 8.40.1