Other Parts Discussed in Thread: CC2650
Hi
I am using CCS 9.1, TI-RTOS for C13XX and C26XX vers 2.21.1.08 on Linux Mint 18 and the XDS110 Debug Probe
I installed the example uartecho_CC2650STK_TI and configured a terminal program with the settings specified in the README.md:
Baud-rate: 9600
Data bits: 8
Stop bits: 1
Parity: None
Flow Control: None
But there is no communication in either sens. I noticed that uart of CC2650 receives garbage, the call to
UART_read(uart, &input, 1);
doesn't block as it should in absense of inbound trafic.
Does the JTAG mode supports access to the uart on the chip ?
With other microcontrollers I have used SWD Mode rather than JTAG mode but the former doesn't work with the CC2650STK .
Can I connect to the onboard uart with the XDS110 ?
Thanks
Peter