Hi all,
I am using the CC2564CMSP432BTBLESW Bluetopia SW stack with the development system described here (ti.com/lit/ug/swru497/swru497.pdf) and I am able to connect and Source audio to several devices. However when I try too connect to two devices in particular, I am unable to. There is no indication as to why - just an "Unknown Error".
Device 1 (Sound Logic XT cylindrical speaker tower):
A3DP+SRC>GetRemoteName 2
GAP_Query_Remote_Device_Name success.
A3DP+SRC>
BD_ADDR: 0x115802980238.
Name: SL TOWER SPKR.
A3DP+SRC>OpenStream 2
AUD_Open_Remote_Stream success.
A3DP+SRC>
atLinkKeyRequest requested: 0x115802980238
A3DP+SRC>
atIOCapabilityRequest requested: 0x115802980238. Responding with IO Capabilities & MITM & OOB.
A3DP+SRC>
atIOCapabilityResponse: 0x115802980238
Capabilities: No Input/Output, no MITM, no Out Of Band (OOB) Data
A3DP+SRC>
atUserConfirmationRequest: 0x115802980238
Auto Accepting authentication: 588737
A3DP+SRC>atSecureSimplePairingComplete authentication event notification.
A3DP+SRC>
atLinkKeyCreation: 0x115802980238
Link Key (16 chars): f6a430fd286b156dc7bfab8f9ddc4
Link Key Stored.
A3DP+SRC>
atAuthenticationStatus: 0 (0 is success) for 0x115802980238
A3DP+SRC>
etEncryption_Change_Result for 0x115802980238, Status: 0x00, Mode: Enabled.
A3DP+SRC>
etAUD_Signalling_Channel_Open_Indication
BD_ADDR: 0x115802980238
A3DP+SRC>
etAUD_Stream_Open_Confirmation
Status: 3 (TIMEOUT is 1, REFUSED is 2, UNKNOWN_ERROR is 3)
BD_ADDR: 0x115802980238
Connection to 0x115802980238 failed.
Device 2 (Apple iMac with BT System Preference open ready to pair):
A3DP+SRC>GetRemoteName 3
GAP_Query_Remote_Device_Name success.
A3DP+SRC>
BD_ADDR: 0x38F9D3C1A043.
Name: My iMac.
A3DP+SRC>OpenSink 3
AUD_Open_Remote_Stream success.
A3DP+SRC>
atLinkKeyRequest requested: 0x38F9D3C1A043
A3DP+SRC>
atIOCapabilityRequest requested: 0x38F9D3C1A043. Responding with IO Capabilities & MITM & OOB.
A3DP+SRC>
atIOCapabilityResponse: 0x38F9D3C1A043
Capabilities: Display Yes/No, no MITM, no Out Of Band (OOB) Data
A3DP+SRC>
atUserConfirmationRequest: 0x38F9D3C1A043
Auto Accepting authentication: 862221
A3DP+SRC>atSecureSimplePairingComplete authentication event notification.
A3DP+SRC>
atLinkKeyCreation: 0x38F9D3C1A043
Link Key (16 chars): defe31a171c6366a01a413c6cf67d7c
Link Key Stored.
A3DP+SRC>
atAuthenticationStatus: 0 (0 is success) for 0x38F9D3C1A043
A3DP+SRC>
etEncryption_Change_Result for 0x38F9D3C1A043, Status: 0x00, Mode: Enabled.
A3DP+SRC>
etAUD_Signalling_Channel_Open_Indication
BD_ADDR: 0x38F9D3C1A043
A3DP+SRC>
etAUD_Stream_Open_Confirmation
Status: 3 (TIMEOUT is 1, REFUSED is 2, UNKNOWN_ERROR is 3)
BD_ADDR: 0x38F9D3C1A043
Connection to 0x38F9D3C1A043 failed.
Any idea why these two devices might be failing an audio stream connection?
Thanks
-Kevin