Hi. The datasheet for the CC256x states in 1.4:
"The following technologies and assisted modes cannot be used simultaneously with the coprocessor: Bluetooth low energy, assisted HFP 1.6 (WBS), and assisted A2DP. Only one technology or assisted mode can be used at a time."
Is it possible to switch between BLE and assisted A2DP / HFP at run-time (without a power cycle and loading the appropriate script)? E.g. use BLE to scan for devices and then connect via BR/EDR and enable assisted A2D? PIf yes, how?
Thanks,
Matthias, BlueKitchen GmbH